Clone a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clone a project

Jump to solution
2,570 Views
juliancox
Contributor V

I have a completed and working project, but I need to create another version of it and the changes are too great to use conditional directives. I would like to create a second project with a different name in the same workspace such that the second project is an exact clone of the first. I would then make the changes to the second project. I assume that I can't just make a copy of the first project's folder

0 Kudos
Reply
1 Solution
2,402 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Julian,

OK, if there is problem, please contact us without any hesitate.

BR

Alice

View solution in original post

0 Kudos
Reply
3 Replies
2,402 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox,

 I was wondering why you think can't copy the first project.

I think you can , just change project name , the name of executable file also can changed as below:

pastedImage_1.png

Could you please tell me the issue when you copy it.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,402 Views
juliancox
Contributor V

Hello Alice,

I don't have a problem as I have not yet tried to copy it. I was just worried that I would lose the the settings or something. I will try later. 

0 Kudos
Reply
2,403 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Julian,

OK, if there is problem, please contact us without any hesitate.

BR

Alice

0 Kudos
Reply