Clone a project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,568件の閲覧回数
juliancox
Contributor V

I have a completed and working project, but I need to create another version of it and the changes are too great to use conditional directives. I would like to create a second project with a different name in the same workspace such that the second project is an exact clone of the first. I would then make the changes to the second project. I assume that I can't just make a copy of the first project's folder

タグ(2)
0 件の賞賛
返信
1 解決策
2,400件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Julian,

OK, if there is problem, please contact us without any hesitate.

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,400件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox,

 I was wondering why you think can't copy the first project.

I think you can , just change project name , the name of executable file also can changed as below:

pastedImage_1.png

Could you please tell me the issue when you copy it.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,400件の閲覧回数
juliancox
Contributor V

Hello Alice,

I don't have a problem as I have not yet tried to copy it. I was just worried that I would lose the the settings or something. I will try later. 

0 件の賞賛
返信
2,401件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Julian,

OK, if there is problem, please contact us without any hesitate.

BR

Alice

0 件の賞賛
返信