Cannot Not Run Free Version of CodeWarrior Development Studio for Microcontrollers V6.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot Not Run Free Version of CodeWarrior Development Studio for Microcontrollers V6.3

12,317件の閲覧回数
Sid_311
Contributor I

I've downloaded CW (I assume its the free version). I had Windows Vista Home Premium 32bit and it ran ok. But since then my hard drive died and had to get a new one, which I loaded with Windows 7 Ultimate 64bit.

 

Of course CW would not install, however I downloaded Windows Virtual PC, along with Windows XP Mode.

 

I installed CW in Virtual PC XP Mode, but when I try to run it, either in XP Application Mode through Windows 7 or the complete virtualization of Windows XP, I am shown a license error:

 

"No valid license key was found for this installation of CodeWarrior Development Studio..."

"Cannot checkout an uncounted license within a Windows Terminal Service guest session."

"Feature: Win32_CWIDE_Limited"

"FLEXnet Licensing error: -103,577"

 

I am a student and we use the Dragon Learner Board (HCS12 Microcontroller) at my University. I would like to have CW running as soon as possible.

 

Thanks in advance.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
12 返答(返信)

6,879件の閲覧回数
looxonline
Contributor I

I would submit a request if the site would let me:

 

Unexpected Error   An unexpected error has occurred. This system may be temporarily unavailable due to technical difficulties. Please go back and try your request again.
If the problem persists, contact our Technical Helpline via phone:
    Americas      1-800-521-6274      6AM-5PM Mountain Standard Time   Europe       9AM-5PM Central European Time        English +44 1296 380 456          German +49 89 92103 559          French +33 1 69 35 48 48     Asia        Asia Pacific +800 2666 8080 9AM-6PM Hong Kong time        China mainland 800 990 8188 9AM-6PM Hong Kong time        Hongkong 2666 8080 9AM-6PM Hong Kong time        India 000 800 852 1155 9AM-6PM Hong Kong time        Japan 0120 191 014 8AM-5PM Tokyo time        Or you can contact us by email at [email protected]

Exception Type: Freescale eBusiness Exception (major: 90000 minor: 0 details: null).
Date: Thu Jan 21 05:22:29 MST 2010
 

 

0 件の賞賛
返信

6,879件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you try the link below?

 https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

This one is working fine as far as I know.

If you are still unable to access it then you might have a problem with your computer. Can you try on another PC?

 

CrasyCat

0 件の賞賛
返信

6,879件の閲覧回数
looxonline
Contributor I

Hi I am having the same problem.

 

The license file that has been provided works but my code size has breached 32k and I am almost done so I am using an evaluation license for a short while. Unfortunately my evaluation license throws the same error.

 

Please could someone have a look and see if it can be fixed.

 

Thanks. 

0 件の賞賛
返信

6,879件の閲覧回数
CrasyCat
Specialist III

Hello

 

Please submit a service request to get one of our licensing people looking into that.

 

CrasyCat

0 件の賞賛
返信

6,879件の閲覧回数
CrasyCat
Specialist III

Hello

 

Can you please post the licence.dat file you have in your installation directory?

 

CrasyCat

0 件の賞賛
返信

6,879件の閲覧回数
sskuce
Fresh Out Contributor

I've got the same exact problem.  I'm migrating to a new Windows 7 Professional 64-bit machine, and CodeWarrior 6.3 Special Edition won't install, so I try Microsoft's "XP Mode" virtualization, and that lets it install, but then I get the license error when I try to run it.  Here's the contents of my license file:

 

INCREMENT Win32_CWIDE_Limited metrowks 5.900 permanent uncounted \
    A43A60C145AF VENDOR_STRING="CodeWarrior IDE 4.2 or later, \
    Windows" HOSTID=ANY
INCREMENT HI100100 metrowks 6.000 permanent uncounted 4F3A93A88E5A \
    VENDOR_STRING="32768 bytes of code, HC08 Compiler ANSI-C" \
    HOSTID=ANY
INCREMENT HI100150 metrowks 6.000 permanent uncounted DF634DEF9BA8 \
    VENDOR_STRING="32768 bytes of C code, 1024 bytes of C++ code, \
    HC08 Linker" HOSTID=ANY
INCREMENT HI405294 metrowks 6.000 permanent uncounted 69552AF534DF \
    VENDOR_STRING="32768 bytes of code, HC08 ANSI-C Debug" \
    HOSTID=ANY
INCREMENT HI409284 metrowks 6.000 permanent uncounted 5649AD2C5DBD \
    VENDOR_STRING="65536 bytes of code, Coldfire C Debug" \
    HOSTID=ANY
INCREMENT Win32_ColdFire_Compiler metrowks 6.0 permanent uncounted \
    CA8F37747B64 VENDOR_STRING="ColdFire Compiler" HOSTID=ANY
INCREMENT Win32_ColdFireV1_Special_64 metrowks 6.0 permanent \
    uncounted 23EF4317B72F VENDOR_STRING="ColdFire Special Edition \
    Compiler" HOSTID=ANY
INCREMENT ProcessorExpertHC08 metrowks 1.000 permanent uncounted \
    2E86E7EC1BC2 VENDOR_STRING="Basic \
    beans;3BB9A2004454C1C59475110BC0E35B7C" HOSTID=ANY
 

 

This is kind of ridiculous Freescale.  64 bit machines have been out forever now, and apparently there's not even a workaround available for users of the special edition.  I realize we're "cheap" for using the free version, but we are at least developing on your hardware.  Without the free development tools, I may as well look to other micro vendors for future projects.

0 件の賞賛
返信

6,879件の閲覧回数
RastislavMatula
Contributor I

Hi,

 

I am using the CW same way, I don't know where can be the problem. Before some time I upgraded to windows seven x64 and I installed windows XP mode. I have installed CW Special Edition for Microcontrollers (downloaded from Freescale web). And everything is working fine...

 

Try to download the latest version (or vice-versa: some older one :smileytongue:) and reinstall it. While there is at least mine working, there have to be way to install it somehow... 

0 件の賞賛
返信

6,879件の閲覧回数
sskuce
Fresh Out Contributor

Hi Ratislav,

 

What version do you have installed?

0 件の賞賛
返信

6,879件の閲覧回数
CrasyCat
Specialist III

Hello

 

Can you try with the attached license file instead?

 

Just rename the file license.dat and copy it in your CodeWarrior installation directory.

 

CrasyCat

0 件の賞賛
返信

6,879件の閲覧回数
ChrisN
Contributor II

Catherine,

I was unable to resolve it any other way. Do you still have the license.dat file?

Thanks,

Chris

https://community.nxp.com/message/310198/edit" style="font-style: inherit; font-family: inherit; col...

0 件の賞賛
返信

6,879件の閲覧回数
ChrisN
Contributor II

I am having the same problem and would like to try the license file you provided but it is no longer attached, probably because this issue is pretty old. Could you dig it up and re-attach or send it to me directly?

Thanks,

Chris

0 件の賞賛
返信

6,879件の閲覧回数
sskuce
Fresh Out Contributor

That worked.  Thanks!

 

Freescale still needs to allow CodeWarrior to install on 64-bit machines, though.  In a few years, it will probably become difficult to get a legal copy of a 32-bit Windows OS.

0 件の賞賛
返信