Can a library created with GCC C be used in a project using Freescale C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can a library created with GCC C be used in a project using Freescale C?

ソリューションへジャンプ
2,130件の閲覧回数
gorakk
Contributor IV

Can a library created with CodeWarrior and GCC C be used in a project using CodWarrior and Freescale C?

 

We are evaluating a third-party library that compiles when using CodeWarrior 10.5 and the GCC C compiler but not with the Freescale C compiler.  Our existing application is using CodeWarrior 10.5 and the Freescale C compiler.

 

There are still issues with the library so before I put any more time into it - can this be successful?  Will a GCC C compiled library work with a Freescale C compiled project?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,921件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

No. the lib made from Gcc compiler can not work for Fresscale ARM compiler.

========================================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Zhang Jun

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,921件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

what chip and CW version do you work with?

Best Regards,

Zhang Jun

0 件の賞賛
返信
1,921件の閲覧回数
gorakk
Contributor IV

We are using the MK61FN1M0VMJ12 and Codewarrior 10.5

Regards,

Allen

0 件の賞賛
返信
1,922件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

No. the lib made from Gcc compiler can not work for Fresscale ARM compiler.

========================================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Zhang Jun

0 件の賞賛
返信