Can a library created with GCC C be used in a project using Freescale C?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can a library created with GCC C be used in a project using Freescale C?

Jump to solution
2,114 Views
gorakk
Contributor IV

Can a library created with CodeWarrior and GCC C be used in a project using CodWarrior and Freescale C?

 

We are evaluating a third-party library that compiles when using CodeWarrior 10.5 and the GCC C compiler but not with the Freescale C compiler.  Our existing application is using CodeWarrior 10.5 and the Freescale C compiler.

 

There are still issues with the library so before I put any more time into it - can this be successful?  Will a GCC C compiled library work with a Freescale C compiled project?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,905 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

No. the lib made from Gcc compiler can not work for Fresscale ARM compiler.

========================================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Zhang Jun

View solution in original post

0 Kudos
Reply
3 Replies
1,905 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

what chip and CW version do you work with?

Best Regards,

Zhang Jun

0 Kudos
Reply
1,905 Views
gorakk
Contributor IV

We are using the MK61FN1M0VMJ12 and Codewarrior 10.5

Regards,

Allen

0 Kudos
Reply
1,906 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

No. the lib made from Gcc compiler can not work for Fresscale ARM compiler.

========================================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Zhang Jun

0 Kudos
Reply