CW4.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,907件の閲覧回数
daistar
Contributor I
how long will i get a copy of CW4.6 evaluation copy????
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,870件の閲覧回数
CrasyCat
Specialist III
Hello
 
Did you order a CD and are you waiting for the CD or are you waiting for a license?
 
You should be able to download the software from the web.
Go to the CodeWarrior for HC12 product page
And download the special edition.
 
Software comes with a special edition allowing you to process up to 32K of C source code.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,871件の閲覧回数
CrasyCat
Specialist III
Hello
 
Did you order a CD and are you waiting for the CD or are you waiting for a license?
 
You should be able to download the software from the web.
Go to the CodeWarrior for HC12 product page
And download the special edition.
 
Software comes with a special edition allowing you to process up to 32K of C source code.
 
CrasyCat
0 件の賞賛
返信
1,871件の閲覧回数
J2MEJediMaster
Specialist I
I don't really understand what you want from such a brief question. I'll try to answer anyway. You can go get the CodeWarrior HCSX(12) page here and follow the Special Edition link to download an evaluation copy of CW 4.6. (I'm assuming you're wanting to use HCS12(X), based on the version number.) Don't forget to downoad the license file, which is typically good for 30 days. Study the charts on that page to understand what the limitations of the Special Edition are before downloading.

---Tom



Message Edited by J2MEJediMaster on 2007-05-29 07:45 AM