CW problem: Lauching name_project_FLASH_OpenSDA has encountered a problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW problem: Lauching name_project_FLASH_OpenSDA has encountered a problem

25,478 Views
matheusnogueira
Contributor I

Hello!

 

I am using the freescale FRDM-KL46Z board with CodeWarrior.

Everytime I try to debug a code this problem happen:

"Lauching name_project_FLASH_OpenSDA has encountered a problem.... the CodeWarrior debugger does not have a Machine Object that supports executable"

and

"The connection with the debugger was interrupted, probably due to a crash

description: "CORBA connection error

Details: "Connection test failed. Reason: org.omg.CORBA.COMM_FAILURE:   vmcid: SUN  minor code: 201  completed: No".

 

I am running the CW in the windows 8.

Does someone know how to fix this problem?

 

Once I did find much information about it, I tried somethings:

I switched the board and still have the problem,

I uninstaller and installed and still have the problem

 

 

I would appreciate any help.

 

Matheus

Labels (1)
0 Kudos
Reply
1 Reply

25,245 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello,

please check if this article can help you:

Killing Me Softly: Zombies and Debugger Engines | MCU on Eclipse


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply