Using PC-Lint on codewarrior 10.6.4 for kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using PC-Lint on codewarrior 10.6.4 for kinetis

2,278 Views
kaustubhkagalka
Contributor II

Hi All,

 

I am having difficulty configuring PC-Lint for our project. We are using MKL26Z256VLH4 controller, has anybody used PC-lint on this controller? I tried follwoing Eclipse and PC-lint: Linticator | MCU on Eclipse, but it does not have any info about how to configure PC-Lint.

 

Any info on how to configure is much appreciated.

 

KK.

Labels (1)
0 Kudos
Reply
1 Reply

1,935 Views
trytohelp
NXP Employee
NXP Employee

Hi,

You can refer to the links:

  1. http://mcuoneclipse.com/2012/04/10/linting-without-a-plugin/
  2. http://mcuoneclipse.com/2012/04/01/eclipse-and-pc-lint-linticator/

Sometimes ago I've performed some tests on PCLint under Eclipse too.

See attached more details and example based on MCU V10.4 and HCs08


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply