CW for MCU v10.1 - inscrutable error message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for MCU v10.1 - inscrutable error message

Jump to solution
2,269 Views
robmilne
Contributor II

I find the UI terribly non-user friendly.  I can't seem to do the simple task of flashing and debugging a S08 project with my P&E usb multilink (rev c, v5.84).  I did manage to initially flash and debug after dealing with a 'launch' issue (?), but I cannot flash the mcu again.  The error message I get is...

 

Error creating session: The CodeWarrior debugger does not have a Machine object that supports the executable.; Internal Error
The CodeWarrior debugger does not have a Machine object that supports the executable.; Internal Error

 

I haven't a clue what this means.

 

-rob

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,640 Views
robmilne
Contributor II

Nevermind - I've gone back to the 'just works' classic 6.3 solution.  The UI may not be sexy but it is more intuitive.

View solution in original post

0 Kudos
Reply
4 Replies
1,641 Views
robmilne
Contributor II

Nevermind - I've gone back to the 'just works' classic 6.3 solution.  The UI may not be sexy but it is more intuitive.

0 Kudos
Reply
1,640 Views
Kaare
Contributor III

Please unmark your last reply as the solution.

 

Going back to an older version, which by the way can't run on 64-bit windows, is NOT a solution the problem you described. I have the exact same problem.

 

I hate the error messages in eclipse. They are almost always a worthless pile of fancy words which gives no help at all.

0 Kudos
Reply
1,640 Views
hefner
Contributor I

 

"...CodeWarrior debugger does not have a Machine object that supports the executable"

 

This happened to me right after I ran a utility to delete all unused FTDI virtual com ports.  All the FTDI devices still work fine, but it seems that the PE Micro USB Multilink Interface doesn't want to play anymore.

 

Amen to the note on eclipse error messages.  Most of them look like a random selection of English words thrown together with no intention of saying anything.  I guess this is what we get for allowing large corporations to use labor in non-English speaking countries instead of good old American engineers (a lot of whom are unemployed these days).

 

Does anyone from Freescale ever monitor these forums?  Does anyone know how to fix this problem?  In English?

0 Kudos
Reply
1,640 Views
J2MEJediMaster
Specialist I

It sounds like that utility might have deleted the Jungo driver, which the P&E mulitlink requires to function. Try checking this forum https://community.freescale.com/message/93204#93204 for how to fix this problem.

 

---Tom

 

 

0 Kudos
Reply