Hi Kirian,
I've installed the MCU V10.5 and Freescale MQX™ RTOS 4.0.0.
after to have launched Eclipse I "drag and drop" the
\Freescale_MQX_4_0\config\twrk60d100m\cw10\twrk60d100m.wsd
file to Eclipse.
I build all projects to rebuild the libraries.
Now I've created a project example via:
File ¦ New ¦ MQX 4.0 Project
then select TWRK60D100M board + "Basic examples ¦ hello"
For ARM Build Tools, there are Gcc or Freescale.
I selected Freescale and Connections "Open source Jtag"
I build the project and launched the debugger.
the application is loaded on-board without problem.
Regards
Pascal