CW Access Paths & function calls

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW Access Paths & function calls

Jump to solution
3,045 Views
UtopiaTim
Contributor III
Hi all,
 
I am incorporating a commercial software package into my project,
and there are over 45 files located in a ...\project\Sources\common
directory.  In these files lie most of the functions that do the 'real' work.
 
To be able to call one of these functions, do I actually have to have
all of the files open under the 'sources' window in Code Warrior, or
is there a way to get the compiler/linker to actually search within
each of these files for the function? 
 
The directory (common) is setup as one of the paths in the Standard
Settings/Access Paths.
 
Since I'm pretty new to doing C things, I figure there might be a way
to do this without putting all of the files open in 'sources'.
 
(also i think that the eval version of CW only lets you have 30 files
open anyway).

Thanks!
 
Tim
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,143 Views
bigmac
Specialist III
Hello Tim,
 
My understanding is that, since the introduction of CW 6.0, the file limit no longer applies to the special edition.
 
Regards,
Mac
 

View solution in original post

0 Kudos
Reply
2 Replies
2,144 Views
bigmac
Specialist III
Hello Tim,
 
My understanding is that, since the introduction of CW 6.0, the file limit no longer applies to the special edition.
 
Regards,
Mac
 
0 Kudos
Reply
2,143 Views
UtopiaTim
Contributor III
Hi Mac,
 
Thanks for the info.  I've just gone above 30 & was wondering what was gonna crash!
 
Figured out how to do things with their code, & am now progressing.

Thanks again,
 
Tim
0 Kudos
Reply