CW Access Paths & function calls

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW Access Paths & function calls

ソリューションへジャンプ
3,173件の閲覧回数
UtopiaTim
Contributor III
Hi all,
 
I am incorporating a commercial software package into my project,
and there are over 45 files located in a ...\project\Sources\common
directory.  In these files lie most of the functions that do the 'real' work.
 
To be able to call one of these functions, do I actually have to have
all of the files open under the 'sources' window in Code Warrior, or
is there a way to get the compiler/linker to actually search within
each of these files for the function? 
 
The directory (common) is setup as one of the paths in the Standard
Settings/Access Paths.
 
Since I'm pretty new to doing C things, I figure there might be a way
to do this without putting all of the files open in 'sources'.
 
(also i think that the eval version of CW only lets you have 30 files
open anyway).

Thanks!
 
Tim
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,271件の閲覧回数
bigmac
Specialist III
Hello Tim,
 
My understanding is that, since the introduction of CW 6.0, the file limit no longer applies to the special edition.
 
Regards,
Mac
 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,271件の閲覧回数
bigmac
Specialist III
Hello Tim,
 
My understanding is that, since the introduction of CW 6.0, the file limit no longer applies to the special edition.
 
Regards,
Mac
 
0 件の賞賛
返信
2,271件の閲覧回数
UtopiaTim
Contributor III
Hi Mac,
 
Thanks for the info.  I've just gone above 30 & was wondering what was gonna crash!
 
Figured out how to do things with their code, & am now progressing.

Thanks again,
 
Tim
0 件の賞賛
返信