CW 11.1 Error - Error initializing Debug Database.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 11.1 Error - Error initializing Debug Database.

Jump to solution
3,402 Views
kaspt
Contributor II

When opening a new empty workspace Code warrior dumps the error:

Error initializing Debug Database.

Could not load debug database. This is indication of an installation or configuration problem. Please contact customer support.

CodeWarrior for MCU  Version: 11.1  Build Id:181224

There was allready a similar issue with a previes version. 

CW 10.5 Error - "Debug Database Initialization" - NXP Community 

But there is no solution that works for me. 

This present’s me from debugging and flashing applications. Diagnostic report attached. 

0 Kudos
Reply
1 Solution
3,344 Views
kaspt
Contributor II

I installed code warrior under a different path (not the default one) now it works.

View solution in original post

0 Kudos
Reply
2 Replies
3,381 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @kaspt ,

Thanks for your post. Are you logging on Windows with Administrator right?  Could you please install the CodeWarrior under the default path?

C:\Freescale\CW MCU v11.1

Or you can also try the method in the following post:

Help with the "Debug Database Initialization" message? - NXP Community

Download the "Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)" from Microsoft and repair the package that was installed with CW to see if it works.


Best Regards
Celeste
--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
--------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,344 Views
kaspt
Contributor II

I installed code warrior under a different path (not the default one) now it works.

0 Kudos
Reply