CW 10.4 compiler/linker bug when copying project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.4 compiler/linker bug when copying project

1,917 Views
alager
Contributor II

I have a coldfire V2 project that compiles and runs fine.

I then followed the "How to copy a CW 10 project" http://mcuoneclipse.com/2012/10/21/copy-my-codewarrior-project/

but the new project, in the same workspace, compiles or links incorrectly, creating a run time exception.

See the image, on the left the code should call tickDriverInit() at address 0x1000040e, but the disasembly shows the jsr to some other "random" address, which causes a run time exception.

5361_5361.pngcw10.4_compiler_bug.png

 

I verified that the original project has the correct code in the disassembly view.  Why is this happening, how to I fix it?

I've been over the compiler, link and assembler settings with a fine toothed comb, and can not find any differences.  What am I missing?

 

Let me know what other info might be needed to track this down.

Thanks,

Aaron

 

UPDATE: Building an identical project from scratch works just fine, but making copies produces the above error.

Labels (1)
0 Kudos
Reply
4 Replies

1,711 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Aaron,

have you tried with a new project? The result is the same? If you are able to clone a new project without problems I recommend to compare both projects settings.

if your rpoblem persists please submit a Service Request with the steps to reproduce the problem. You can reach us at www.freescale.com/support?

Best regards,

Carlos


1,711 Views
alager
Contributor II

I have three projects total in the same workspace.  The original project (A), the copy of A, (B), and a build from the ground up copy (C).  All three projects compile without error or warnings, all three projects have the same compiler settings (at least as far as I can see after spending a week looking over those check boxes and drop downs).  Project A and C can be run in the debugger without error indefinitely.  Project B runs until it hits the line shown in the image above, then throws an illegal op-code exception.

All three projects are in SVN, and I tried doing a comparison between URLs, and there were a surprising number of differences, which I did not expect, but I didn't see anything that would lead me to an error like above.

0 Kudos
Reply

1,711 Views
trytohelp
NXP Employee
NXP Employee

Hi Aaron,

this is just to know what is the status of this problem.

is it solved or under investigation via Service Request process ?

Don't hesitate to contact us.

Regards

Pascal

0 Kudos
Reply

1,711 Views
alager
Contributor II

I'm going to start a service request after typing this.  ALL my projects in my workspace quit working yesterday evening....I'm really getting frustrated with this IDE.

0 Kudos
Reply