CW 10.3 install - Error decompressing data! Corrupted installer?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.3 install - Error decompressing data! Corrupted installer?

ソリューションへジャンプ
5,133件の閲覧回数
bowerymarc
Contributor V

I'm attempting to install CW 10.3 to a windows XP SP2 machine with no luck.

Trying both the offline and online installer.

It will get to a certain point and give me the error:  Error decompressing data! Corrupted installer?

Usually it's when extracting doc.zip but sometimes another file.  NOTE: that is with the online installer (after it downloads stuff and starts unpacking).

With the offline installer it gets part of the way and then I get (always) this error (pop-up):  7-Zip: Data error.

I have plenty of disk space, my C drive is NTFS, system is normal otherwise.

I tried also installing on a windows XP SP2 partition using Parallels 7 on the mac, and get the same kind of error!

The installer doesn't leave any hints in the system Event Viewer, not sure how to debug it.

Regards,
Marc

ラベル(1)
0 件の賞賛
返信
1 解決策
3,317件の閲覧回数
bowerymarc
Contributor V

it looks like my ISP, Time Warner Cable of New York, is doing something to my downloads.  Using the same computer (laptop) in a different location, I was able to download the offline installer and successfully install.

I had an issue with them a couple of years ago where they were blocking Freescale's site specifically for some reason, once I logged in (not as anonymous).

Apparently they are doing some kind of stateful packet inspection which is corrupting the CW archive.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,318件の閲覧回数
bowerymarc
Contributor V

it looks like my ISP, Time Warner Cable of New York, is doing something to my downloads.  Using the same computer (laptop) in a different location, I was able to download the offline installer and successfully install.

I had an issue with them a couple of years ago where they were blocking Freescale's site specifically for some reason, once I logged in (not as anonymous).

Apparently they are doing some kind of stateful packet inspection which is corrupting the CW archive.

0 件の賞賛
返信