CW 10.3 install - Error decompressing data! Corrupted installer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.3 install - Error decompressing data! Corrupted installer?

Jump to solution
5,126 Views
bowerymarc
Contributor V

I'm attempting to install CW 10.3 to a windows XP SP2 machine with no luck.

Trying both the offline and online installer.

It will get to a certain point and give me the error:  Error decompressing data! Corrupted installer?

Usually it's when extracting doc.zip but sometimes another file.  NOTE: that is with the online installer (after it downloads stuff and starts unpacking).

With the offline installer it gets part of the way and then I get (always) this error (pop-up):  7-Zip: Data error.

I have plenty of disk space, my C drive is NTFS, system is normal otherwise.

I tried also installing on a windows XP SP2 partition using Parallels 7 on the mac, and get the same kind of error!

The installer doesn't leave any hints in the system Event Viewer, not sure how to debug it.

Regards,
Marc

Labels (1)
0 Kudos
Reply
1 Solution
3,310 Views
bowerymarc
Contributor V

it looks like my ISP, Time Warner Cable of New York, is doing something to my downloads.  Using the same computer (laptop) in a different location, I was able to download the offline installer and successfully install.

I had an issue with them a couple of years ago where they were blocking Freescale's site specifically for some reason, once I logged in (not as anonymous).

Apparently they are doing some kind of stateful packet inspection which is corrupting the CW archive.

View solution in original post

0 Kudos
Reply
1 Reply
3,311 Views
bowerymarc
Contributor V

it looks like my ISP, Time Warner Cable of New York, is doing something to my downloads.  Using the same computer (laptop) in a different location, I was able to download the offline installer and successfully install.

I had an issue with them a couple of years ago where they were blocking Freescale's site specifically for some reason, once I logged in (not as anonymous).

Apparently they are doing some kind of stateful packet inspection which is corrupting the CW archive.

0 Kudos
Reply