CRC Calculation for HCS08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CRC Calculation for HCS08

2,343 次查看
preetuabraham
Contributor III

I would like to know the CRC calculation for MC9S08AC128 pagine meory devices .Whether the CRC should be calculated for all the pages or it is enough to calculate the CRC for only the memory ranges where code is allocated . I am storing the Final value at location 0xfFFC0 .The memory ranges are as shown below to calculate the CRC

 

 

1)First block of memory: 0x20F0 to 0x7FFF

 

2)Second block of memory :0x8000 to 0xBFFF

3)Third block of memory : 0xC000 to 0xff9b

4) fourth block of memory : 0xFFCC to 0xFFFF

5)Last Block : 0x28000 to 0x2bFFF

 

 

I had the linker file for my project as below:

 

SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */
    MY_STK                   =  NO_INIT      0x15FF TO 0x17FF;
    RAM1                     =  READ_WRITE   0x0080 TO 0x01FF;
    RAMSEG                   =  READ_WRITE   0x0200  TO 0x0370;
    RAM2                     =  READ_WRITE   0x0372 TO 0x15FE;
    RAM3                     =  READ_WRITE   0x1870 TO 0x20EF;
    ROM                      =  READ_ONLY    0x20F0 TO 0x7FFF;
    ROM1                     =  READ_ONLY    0xC000 TO 0xFF9B;
    /* banked FLASH ROM */
    PPAGE_0                  =  READ_ONLY    0x008000 TO 0x00BFFF; /* PAGE partially contained in ROM segment */
    PPAGE_2                  =  READ_ONLY    0x028000 TO 0x02Bfff;
    //PPAGE_4                  =  READ_ONLY    0x048000 TO 0x04BFFF;
    //PPAGE_5                  =  READ_ONLY    0x058000 TO 0x05BFFF;
    //PPAGE_6                  =  READ_ONLY    0x068000 TO 0x06BFFF;
    //PPAGE_7                  =  READ_ONLY    0x078000 TO 0x07BFFF;
END

PLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */
    MySeg                      INTO  RAM1;
    DEFAULT_RAM                   INTO  RAM2,RAM3;
    DEFAULT_ROM, ROM_VAR, STRINGS INTO  ROM,PPAGE_0,ROM1,PPAGE_2;//PPAGE_4,PPAGE_5,PPAGE_6,PPAGE_7; /* See compiler option -OnB=b. */
    //PAGED_ROM                      INTO  PPAGE_0,ROM1,PPAGE_2,PPAGE_4,PPAGE_5,PPAGE_6,PPAGE_7;    
   SSTACK                        INTO  MY_STK;

标签 (1)
0 项奖励
回复
3 回复数

2,071 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Preetu,

You'd better calculate  the memory rang in one page , do not beyond one page,

the memory rang can small then one page .

Hope it helps
Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,071 次查看
preetuabraham
Contributor III

Hi Alice,

You are mentioning not to calculate the memory range for 0x28000 to 0x2bFFF.But my data gets allocated even for the memory range 0x28000 to 0x2bFFF as per the memory map file. I had given the linker file allocation based on the memory being used by the program

I did not understand which page you are mentioning to calcluate.

0 项奖励
回复

2,071 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Preetu,

The memory you can specify by yourself to calculate CRC.

Also there is a thread , maybe helpful for you.

CRC 8 bits

BR

Alice

0 项奖励
回复