C++ with mqx 3.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C++ with mqx 3.7

Jump to solution
1,154 Views
evgenyerlihman
Contributor IV

Hello All,

 

Has any body been able to use the C++ library, using the BSPCFG_ENABLE_CPP flag, and MQX 3.7 version?

 

Thanks,

Evgeny

Labels (1)
0 Kudos
Reply
1 Solution
944 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Evgeny

There is a known problem in MQX3.7 for C++ examples for Kinetis platform. I would recommend updating to v3.8 or higher version.

Below is extracted from v3.8 release note:

New C++ example application was created and C++ functionality was enabled on all platforms.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
945 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Evgeny

There is a known problem in MQX3.7 for C++ examples for Kinetis platform. I would recommend updating to v3.8 or higher version.

Below is extracted from v3.8 release note:

New C++ example application was created and C++ functionality was enabled on all platforms.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------