C++ with mqx 3.7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

C++ with mqx 3.7

跳至解决方案
1,147 次查看
evgenyerlihman
Contributor IV

Hello All,

 

Has any body been able to use the C++ library, using the BSPCFG_ENABLE_CPP flag, and MQX 3.7 version?

 

Thanks,

Evgeny

标签 (1)
0 项奖励
回复
1 解答
937 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Evgeny

There is a known problem in MQX3.7 for C++ examples for Kinetis platform. I would recommend updating to v3.8 or higher version.

Below is extracted from v3.8 release note:

New C++ example application was created and C++ functionality was enabled on all platforms.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
938 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Evgeny

There is a known problem in MQX3.7 for C++ examples for Kinetis platform. I would recommend updating to v3.8 or higher version.

Below is extracted from v3.8 release note:

New C++ example application was created and C++ functionality was enabled on all platforms.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------