Bookmark Bug: CW IDE v5.9.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bookmark Bug: CW IDE v5.9.0

Jump to solution
2,794 Views
BasePointer
Contributor II
Hi,
 
1. Set a bookmark in your source file by pressing Ctrl+F2
2. Press enter
3. Goto to a few line below by arrow-down key.
4. Set a bookmark again with Ctrl+F2
5. Press enter a few time.
6. Navigate between bookmarks by pressing F2
 
This also sometimes causes IDE to crash.
 
IDE.exe 5.9.0 Build 2330 18.05.2007,03:17.
 
Thank you.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,730 Views
CrasyCat
Specialist III
Hello
 
I did some tests with CodeWarrior MCU V6.0, but I am unabl eto reproduce teh trouble.
 
Anyway, I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat

View solution in original post

0 Kudos
Reply
3 Replies
1,730 Views
CrasyCat
Specialist III
Hello
 
I need more information on this one.
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 Kudos
Reply
1,730 Views
BasePointer
Contributor II
Hi,
 
1. HCS08 / C Project
2. CodeWarrior Development Studio for Microcontrollers V6.0 Release, build 7134-30May07
 
Thanks.
0 Kudos
Reply
1,731 Views
CrasyCat
Specialist III
Hello
 
I did some tests with CodeWarrior MCU V6.0, but I am unabl eto reproduce teh trouble.
 
Anyway, I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 Kudos
Reply