Board Support in new Codewarrior for HC(S)08 Versions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Board Support in new Codewarrior for HC(S)08 Versions

ソリューションへジャンプ
4,221件の閲覧回数
eckhard
Contributor V
Hello,

in CW3.1 for HC08 there was a staionaiy for the QT4 Demoboard that used the User Monitor:
I used this fo a few projects with the Nitron Controllers and the User Monitor.
In the newer Codewarrior Versions for HC(S)08 this board is no longer supported and there seems to be a completely diffenrent structure regarding the stationaries. Is it possible to get Board Support for the Nitron Demo Board or for the Nitron User Monitor ?


Regards Eckhard
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,109件の閲覧回数
CrasyCat
Specialist III
Hello
 
Do not know which is the difference, but I would ^suggest you to submit a service request for that.

Click here to submit a service request.
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,109件の閲覧回数
CrasyCat
Specialist III
Hello
 
The new CodeWarrior for HC08 (V5.x and higher) are not using stationeries any more to create projects, but a wizard. 
 
You should still be able to program the Nitron (QT) board with these release.
 
Either use the wizard to create a project for HC08QTx or in the startup screen you can select "Load Example Project" and select a HC08QTx project from there.
 
A new project (duplicated from the selected demo project will be created and should be set up for the board.
 
I hope this helps.
 
CrasyCat
0 件の賞賛
返信
2,109件の閲覧回数
eckhard
Contributor V
Hello,

the problem is not the HC08 QT/QY controller, the problem is to use the user Monitor.

Eckhard
0 件の賞賛
返信
2,110件の閲覧回数
CrasyCat
Specialist III
Hello
 
Do not know which is the difference, but I would ^suggest you to submit a service request for that.

Click here to submit a service request.
CrasyCat
0 件の賞賛
返信