Board Support in new Codewarrior for HC(S)08 Versions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board Support in new Codewarrior for HC(S)08 Versions

Jump to solution
4,248 Views
eckhard
Contributor V
Hello,

in CW3.1 for HC08 there was a staionaiy for the QT4 Demoboard that used the User Monitor:
I used this fo a few projects with the Nitron Controllers and the User Monitor.
In the newer Codewarrior Versions for HC(S)08 this board is no longer supported and there seems to be a completely diffenrent structure regarding the stationaries. Is it possible to get Board Support for the Nitron Demo Board or for the Nitron User Monitor ?


Regards Eckhard
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,136 Views
CrasyCat
Specialist III
Hello
 
Do not know which is the difference, but I would ^suggest you to submit a service request for that.

Click here to submit a service request.
CrasyCat

View solution in original post

0 Kudos
Reply
3 Replies
2,136 Views
CrasyCat
Specialist III
Hello
 
The new CodeWarrior for HC08 (V5.x and higher) are not using stationeries any more to create projects, but a wizard. 
 
You should still be able to program the Nitron (QT) board with these release.
 
Either use the wizard to create a project for HC08QTx or in the startup screen you can select "Load Example Project" and select a HC08QTx project from there.
 
A new project (duplicated from the selected demo project will be created and should be set up for the board.
 
I hope this helps.
 
CrasyCat
0 Kudos
Reply
2,136 Views
eckhard
Contributor V
Hello,

the problem is not the HC08 QT/QY controller, the problem is to use the user Monitor.

Eckhard
0 Kudos
Reply
2,137 Views
CrasyCat
Specialist III
Hello
 
Do not know which is the difference, but I would ^suggest you to submit a service request for that.

Click here to submit a service request.
CrasyCat
0 Kudos
Reply