Best compiler for MPC5604P microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Best compiler for MPC5604P microcontroller

ソリューションへジャンプ
2,293件の閲覧回数
Firoz
Contributor I

Hello ,

 

I have a licensed version of Codewarrior development studio for HCS12X v4.7. Now i need to do a project on MPC5604P micro. Can you please help me to know the best IDE to work on with MPC5604P family.

 

Also is there any patch for my existing IDE to work on MPC5604P micro?

 

Thanks in advance

 

Regards

Firoz

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,844件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,845件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

0 件の賞賛
返信