Best compiler for MPC5604P microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Best compiler for MPC5604P microcontroller

Jump to solution
2,352 Views
Firoz
Contributor I

Hello ,

 

I have a licensed version of Codewarrior development studio for HCS12X v4.7. Now i need to do a project on MPC5604P micro. Can you please help me to know the best IDE to work on with MPC5604P family.

 

Also is there any patch for my existing IDE to work on MPC5604P micro?

 

Thanks in advance

 

Regards

Firoz

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,903 Views
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

View solution in original post

0 Kudos
Reply
1 Reply
1,904 Views
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

0 Kudos
Reply