Best compiler for MPC5604P microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Best compiler for MPC5604P microcontroller

跳至解决方案
2,340 次查看
Firoz
Contributor I

Hello ,

 

I have a licensed version of Codewarrior development studio for HCS12X v4.7. Now i need to do a project on MPC5604P micro. Can you please help me to know the best IDE to work on with MPC5604P family.

 

Also is there any patch for my existing IDE to work on MPC5604P micro?

 

Thanks in advance

 

Regards

Firoz

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,891 次查看
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,892 次查看
stanish
NXP Employee
NXP Employee

Hi Firoz,

 

Freescale has CodeWarrior for MPC55xx/56xx v2.7 available here:

 

http://cache.freescale.com/lgfiles/devsuites/PowerPC/CW55xx_v2_7_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Deb...

 

So if you used to work with CodeWarrior for S12 IDE  it will be familiar to you.

Plus if you have valid standard or professional CodeWarrior suite license  you can generate also license for CW for MPC55xx.

 

There are also other vendor tools e.g. GreenHills Multi, Diab,....

 

Stanish

0 项奖励
回复