Are there any non-LDD CANBUS componet in Process Expert?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any non-LDD CANBUS componet in Process Expert?

ソリューションへジャンプ
1,607件の閲覧回数
修華許
Contributor III

Cause I can't find any CAN BUS device which is non-LDD

For a non-RTOS user like me, it's confusing to use a LDD device

Do we have to use a LDD device for a CAN BUS component?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,462件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

for kinetis, KDS/Codewarrior also  includes Init_CAN bean can perform CAN module initialization.

for the moment, we don't have other non-LDD CAN component.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,463件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

for kinetis, KDS/Codewarrior also  includes Init_CAN bean can perform CAN module initialization.

for the moment, we don't have other non-LDD CAN component.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,462件の閲覧回数
修華許
Contributor III

Thanks .

Then I don't have to search where the non-LDD CAN BUS is .

I will try init_CAN instead.

0 件の賞賛
返信