Are there any non-LDD CANBUS componet in Process Expert?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any non-LDD CANBUS componet in Process Expert?

Jump to solution
1,534 Views
修華許
Contributor III

Cause I can't find any CAN BUS device which is non-LDD

For a non-RTOS user like me, it's confusing to use a LDD device

Do we have to use a LDD device for a CAN BUS component?

Labels (1)
0 Kudos
Reply
1 Solution
1,389 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

for kinetis, KDS/Codewarrior also  includes Init_CAN bean can perform CAN module initialization.

for the moment, we don't have other non-LDD CAN component.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,390 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

for kinetis, KDS/Codewarrior also  includes Init_CAN bean can perform CAN module initialization.

for the moment, we don't have other non-LDD CAN component.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,389 Views
修華許
Contributor III

Thanks .

Then I don't have to search where the non-LDD CAN BUS is .

I will try init_CAN instead.

0 Kudos
Reply