Abro un proyecto con el CW 10.6 y no me deja agregar componentes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Abro un proyecto con el CW 10.6 y no me deja agregar componentes

跳至解决方案
1,055 次查看
gustavocampos
Contributor I

Tengo instalado el codewarrior 10.6 y cuando abro un proyecto no me deja agregar componentes de la libreria, me aprece en gris.

标签 (1)
0 项奖励
回复
1 解答
923 次查看
TICS_Fiona
NXP Employee
NXP Employee

Whether you can create a new bareboard project in CodeWarrior v10.6 and enable “Processor Expert” option when creating it?  Whether the components are available in the Components Library?

If yes, then the problem is probably concerned with the project, could you please attach an example project to help us reproduce the problem? Thanks!  

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
924 次查看
TICS_Fiona
NXP Employee
NXP Employee

Whether you can create a new bareboard project in CodeWarrior v10.6 and enable “Processor Expert” option when creating it?  Whether the components are available in the Components Library?

If yes, then the problem is probably concerned with the project, could you please attach an example project to help us reproduce the problem? Thanks!  

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复