9s12xge128 with emulated eeprom

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9s12xge128 with emulated eeprom

3,803件の閲覧回数
JohnnyP
Contributor III

My product is based on a 9s12c32.  The user interface is old school, using pots and dip switches.

It's time for a redesign to make it pc compatible, so I need to add EEPROM.

I'm looking at the 9s12XGE128, which uses emulated EEPROM.

How hard is this to use?  How many registers need to be set up to get it going?

タグ(1)
0 件の賞賛
返信
5 返答(返信)

3,688件の閲覧回数
JohnnyP
Contributor III

Jennie:

Thank you for the project files.

I use assembly language.  The code is in one file.

I will try to figure out your main.c code and convert it to assembly.

JohnP

0 件の賞賛
返信

3,688件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Ok, thanks.

unfortunately I don't have same assembly code.

This need to be converted by user self.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,688件の閲覧回数
JohnnyP
Contributor III

Jennie:

Ok.  I don't have any of these on hand yet, but I'll post the code when I get it figured out.

JohnP

0 件の賞賛
返信

3,688件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi John,

Thanks in advance!

Best Regards,

Jennie.

0 件の賞賛
返信

3,688件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi John

My colleague ever made demo code of XEG128 emulate eeprom.

See attached.
Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信