Voltage - 4,97 V
Amplitude impulse - 0 - 5 V
Bus clock - 32 000 000 Hz
This system read pulse data from IR key.
Each team is always initialize the timer and at the end
it turns off and resets. I am put breakpoint on input capture and start. If not work input capture on long time - timer owerflow and work interrupt overflow... After first command, next all commands work input capture and all system work correctly.
THX.