8 Bit MCU SE License

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8 Bit MCU SE License

Jump to solution
2,561 Views
Edusra
Contributor I
Hello
I am a newbie in this forum.
I can't find the link to upgrade the license of CW 5.1 SE to use 16K of Code.
Can anyone help me with this?
Thank you
Edusra
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,665 Views
CrasyCat
Specialist III
Hello
 
Not sure I understand what you are looking for here.
 
CodeWarrior for HC08 V5.1 comes per default with a special edition allowing you to build up to 16K of C source code.
 
So there is no need to register for a special edition.
 
Did you try to build/debug with CW HC08 V5.1? What is happening?
 
CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
1,666 Views
CrasyCat
Specialist III
Hello
 
Not sure I understand what you are looking for here.
 
CodeWarrior for HC08 V5.1 comes per default with a special edition allowing you to build up to 16K of C source code.
 
So there is no need to register for a special edition.
 
Did you try to build/debug with CW HC08 V5.1? What is happening?
 
CrasyCat
0 Kudos
Reply
1,665 Views
J2MEJediMaster
Specialist I
Have you tried the following in the CodeWarrior IDE: Help | Register Product?

---Tom