64 bit classic Code warrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

64 bit classic Code warrior

1,392 Views
chaitanya
Contributor II

Does code warrior classic(version 7.0 or 7.2) work with Windows 10 or Windows 7 64 bit?  Is there a 64 bit version available somewhere?

0 Kudos
Reply
1 Reply

1,344 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi  Chaitanya Athalye

CodeWarrior  classic 7.0 and 7.2 don't support 64bit win10.

To work with 64bit win10, please use CW11.1 instead

CodeWarrior® for Microcontrollers-Eclipse IDE 11.1 | NXP 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply