why when connected to the target, codewarrior debugger continue running,not stop at reset entry? processor is mpc862, with PowerTAP Pro.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why when connected to the target, codewarrior debugger continue running,not stop at reset entry? processor is mpc862, with PowerTAP Pro.

1,871件の閲覧回数
tomlucas
Contributor II

Once connected to the target, codewarrior debugger not stop, and running always.

when click the pause button in codewarrior debugger icon, it give us : CCSProtocolPlugin:Failed to stop process[no connection to the target or target power is off]

 

what may cause this?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,727件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello tom lucas,

Probably there is problem to setup the basic connection.

Would you please capture CCS log in CodeWarrior IDE to me to do more investigation?

Please enable CCS log from "Edit->Debug Version Setting-> Debugger->Remote Debugging->Edit Connection->Enable logging" and connect to the target from Debug->Connect, you will find CCS log in CodeWarrior IDE.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,727件の閲覧回数
tomlucas
Contributor II

thks fr rply!

I view the log , and compare it with other normal working log,find:

  It does not read CCS_reg index 2032, so can not get the entry.

what make the debugger not to read ccs_reg of index 2032?

I do not know the debugger working flow,you can explain it for me in detail?

thks mch!

0 件の賞賛
返信