what is the difference between usb tap and cw tap?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the difference between usb tap and cw tap?

1,793件の閲覧回数
jianminlv
Contributor I

I can use usb tap and cw 10.4 to program nand flash on my board based on 8309  sucessfully, but failed to use cw tap and 10.4, why?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,690件の閲覧回数
Pavel
NXP Employee
NXP Employee

Test connection using the following command sequence:

Connection Server from your Windows' Start->Programs menu.   When the CCS icon appears in the Windows Tooltray, double-click it to bring up the CCS Console.  At the CCS Console prompt, enter these commands and send me your results:

  clear
  show ver
  pwd
  findcc cwtaps -usb
  findcc cwtaps
  source IDcode.tcl
  1   <------  selects your CWTAP via USB connection
  show cc
  scanboard

 

Can CodeWarrior connection server find the CodeWarrior TAP using “findcc” command?

Can codeWarrior TAP detect connection to the MPC8309 board using “scanboard” command?


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,690件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello jianmin lv,

What's the failure, can you please show the error log?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信