CDC Example on MC9s08jm60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CDC Example on MC9s08jm60

1,438件の閲覧回数
elettronicarewo
Contributor I

Hi, I'd like to try the CDC class example (find in USB STACK).I never  use USB and this micro before, so i have a dubt: which XTAL i need to use for run the example as is it? Can i use 4MHz? Anyone can help me to calc the value for set proprery the register?

ラベル(1)
0 件の賞賛
返信
1 返信

1,374件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

regarding the CDC demo code for MC9S08JM60, please use below USB stack v4.1.1:

USB Stack v4.1.1 Freescale bare metal (no OS) USB Stack

Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信