verification of merged s19 files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

verification of merged s19 files

1,030 次查看
santoshkandarka
Contributor I

I have merged two files i.e application and bootloader into single s19 file. I wanted to flash it by codewarrior v10.6 and  debugger if it is working properly.Controller is Kinetis E-series. Flash memory range is 0x0000 to 0x1FFF.

标签 (1)
0 项奖励
回复
1 回复

970 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello santosh,

Yes, you can flash the s19 file into your chip through the "Flash File to target",

Please check the attach video .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复