verification of merged s19 files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

verification of merged s19 files

1,037件の閲覧回数
santoshkandarka
Contributor I

I have merged two files i.e application and bootloader into single s19 file. I wanted to flash it by codewarrior v10.6 and  debugger if it is working properly.Controller is Kinetis E-series. Flash memory range is 0x0000 to 0x1FFF.

ラベル(1)
0 件の賞賛
返信
1 返信

977件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello santosh,

Yes, you can flash the s19 file into your chip through the "Flash File to target",

Please check the attach video .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信