_timer_create_component in one more tasks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

_timer_create_component in one more tasks

ソリューションへジャンプ
1,552件の閲覧回数
norbertoj
Contributor III

Hi, I have the next question.

I have three tasks that need to work with timmers. So, Should I  put_timer_create_component for each task? Or, Do I need just one time in a (main) task?

 

Regardly,

 

Norberto Jiménez

ラベル(1)
0 件の賞賛
返信
1 解決策
1,471件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto Jiménez,

You'd better create three timer on the three tasks .

The task do not use the other tasks source .

Hope it helps

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,472件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto Jiménez,

You'd better create three timer on the three tasks .

The task do not use the other tasks source .

Hope it helps

Alice

0 件の賞賛
返信