tbdml_gdi12.dll not loaded

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tbdml_gdi12.dll not loaded

ソリューションへジャンプ
2,520件の閲覧回数
yunjieli
Contributor I

Driver DLL CWS12v5.1\prog\gdi\tbdml_gdi12.dll or one of its components not found or loaded. System Error 126 when I debug my MC9S12XDP512 in Windows 10. Anyone has idea what this problem is and how to solve it? Thanks.

ラベル(1)
1 解決策
1,931件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Li,

There are some restrictions due to driver limitations for 64 bit on new Windows versions.

You will see more details under the txt files: \CWS12v5.1\Release_Notes\HC12

    Notes_CW_HC12_64bit.txt

    Notes_CW_HC12_Vista.txt

Extract of  Notes_CW_HC12_64bit.txt:

+++++++++++++++++++

Known problems:

--------------

(1) The following connections are not working with 64 bits Windows:

        - USB-ML-12-Rev A

        - USB-ML-12-Rev B

        - Softec - inDart-HCS12

        - TBDML

+++++++++++++++++++


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,932件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Li,

There are some restrictions due to driver limitations for 64 bit on new Windows versions.

You will see more details under the txt files: \CWS12v5.1\Release_Notes\HC12

    Notes_CW_HC12_64bit.txt

    Notes_CW_HC12_Vista.txt

Extract of  Notes_CW_HC12_64bit.txt:

+++++++++++++++++++

Known problems:

--------------

(1) The following connections are not working with 64 bits Windows:

        - USB-ML-12-Rev A

        - USB-ML-12-Rev B

        - Softec - inDart-HCS12

        - TBDML

+++++++++++++++++++


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------