target task greyed out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

target task greyed out

2,066件の閲覧回数
hawk
Contributor II

I am getting the error "Error setting debug context for run configuration Active Debug Context".


Some reading and I came "target configuration", which is greyed out. So I can't check it or change it.


Can anyone help me with the above error. I am using USB Multilink universal to (attempt) to program a MC9SO8AW32.


I have never seen BKGD go low, will check clock now. Ok, found one problem, needed b+ on another trace. Processor running.


But now I have these two new errors: According to the forum, a-lot of people do. Followed the suggestions in those posts and those pins seem ok. BKGD, VDD, Gnd, and reset.


Much Thanks,


David

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,960件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi David,

Please accept my apology for the time delayed to get back to you on this issue, I was heavily backlogged!

regarding this problem, if it still there, then, could you mind upload an screen-shot to here for further investigating?

0 件の賞賛
返信

1,960件の閲覧回数
hawk44
Contributor I

Thank your for your kindness.

Problem resolved, erased, re-flashed.

Thank your for at least replying, I was under pressure to get the job done by xx time and I am new to CodeWarrior,

It was about to drive me nuts, seemed like the simplest things didn't work.

But we got it done, a day ahead of time. :smileyhappy:

Thanks again for your reply. Have a great day and weekend

David

0 件の賞賛
返信