sweep the frequency 1KHz to 2 KHz with constant duty cycle using code warrior V10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sweep the frequency 1KHz to 2 KHz with constant duty cycle using code warrior V10.5

跳至解决方案
2,396 次查看
venkateshgv
Contributor II

Hello,i am using controller s9s08qd4 for i need help how to sweep the frequency 1KHz to 2 KHz with constant duty cycle using code warrior V10.5?

标签 (1)
0 项奖励
回复
1 解答
2,242 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

Are you using Processor Expert ?

Processor Expert allows you to manage the Clock settings and has a feature named Enabled speed modes.

See below:

pastedImage_0.png


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,243 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

Are you using Processor Expert ?

Processor Expert allows you to manage the Clock settings and has a feature named Enabled speed modes.

See below:

pastedImage_0.png


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,242 次查看
venkateshgv
Contributor II

HI.. Pascal Irrle..

Thanks for your answer.

this settings already done.

currently i tried with using processor expert.i can't able to get.

but i need to change the frequency of the output PWM signal with constant duty cycle.

if you have any code without using processor expert.plz share it

i can try with that code.

Have a great day ahead!!!!!!!!

Venkat G V

0 项奖励
回复
2,242 次查看
trytohelp
NXP Employee
NXP Employee

Hi Venkat,

Thanks for the feedback.

Unfortunately I don't have example like that.

I recommend you to post your question to 8-bit Microcontrollers

Pascal

0 项奖励
回复