reading constant from paged memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

reading constant from paged memory

ソリューションへジャンプ
26,525件の閲覧回数
martinlockner
Contributor III

I am using codewarrior 10.4 with a mc9s08dz128 microcontroller. I have the micro set for banked memory and have placed a constant table in paged memory (it starts at 0x58000). I used the following #pragma to locate the table in paged memory:

 

 

#pragma CONST_SEG __FAR_SEG PAGED_ROM

 

extern const byte printer_fonts [] = {

 

My problem is reading one of these constant bytes. In reading the documentation it seems like the compiler/linker will automatically handle the extra addressing needed but nothing I have tried works. If I try to read the first byte I get the value that is located at address 0x8000 which means that the page register is not being handled. Anyone run into similar problems? Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
26,389件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Martin,

please read attached an3730 document and demo code, which includes how to read/write HCS08 paged memory.

Hope this helps!

========================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

ZhangJun

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
26,390件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Martin,

please read attached an3730 document and demo code, which includes how to read/write HCS08 paged memory.

Hope this helps!

========================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信