make (e=5): Access is denied

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

make (e=5): Access is denied

4,980件の閲覧回数
Pascal_BERNARD
NXP Employee
NXP Employee

Hi,

 

When trying to build using Code Warrior 10.6, I get:

 

**** Build of configuration FLASH for project FRDM-KL46Z-PEx-GEN6 ****

"C:\\Freescale\\CW MCU v10.6\\gnu\\bin\\mingw32-make" -j16 all
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-1.bat, C:\Users\R20246\AppData\Local\Temp\make8344-1.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-2.bat, C:\Users\R20246\AppData\Local\Temp\make8344-2.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-3.bat, C:\Users\R20246\AppData\Local\Temp\make8344-3.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-4.bat, C:\Users\R20246\AppData\Local\Temp\make8344-4.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-5.bat, C:\Users\R20246\AppData\Local\Temp\make8344-5.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-6.bat, C:\Users\R20246\AppData\Local\Temp\make8344-6.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-7.bat, C:\Users\R20246\AppData\Local\Temp\make8344-7.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-8.bat, C:\Users\R20246\AppData\Local\Temp\make8344-8.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-9.bat, C:\Users\R20246\AppData\Local\Temp\make8344-9.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-a.bat, C:\Users\R20246\AppData\Local\Temp\make8344-a.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-b.bat, C:\Users\R20246\AppData\Local\Temp\make8344-b.bat, ...) failed.
process_begin: CreateProcess(C:\Users\R20246\AppData\Local\Temp\make8344-c.bat, C:\Users\R20246\AppData\Local\Temp\make8344-c.bat, ...) failed.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.
make (e=5): Access is denied.

 

I have a virtual machine allowing me to work but I can't fix this issue since weeks. I have administrator access on my Computer and we tried a lot already using our IT support.

 

Any suggestions?

 

Thanks,

Pascal

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,700件の閲覧回数
zhifenggu
Contributor I

Hi Pascal

     I use the arm gcc toolchain in the KDS(D:\Program Files\Freescale\KDS 1.1.1\toolchain\bin\make.exe) to bulid my own project(use windows Command prompt to call make.exe ),i got the same issue!

     I google the problem, there are many solutions, but i still got the problem.
     Did you solve the problem?

0 件の賞賛
返信

3,700件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Do you get exactly the same message ?

I've checked in our data base and I don't find request (excepted this one) regarding similar problem.

KDS V2.0 has been released.

You can access it to the link:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE&tid=vanKDS

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信