invalid project path duplicate path entries found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

invalid project path duplicate path entries found

Jump to solution
11,931 Views
kleckerspur
Contributor III

Hello,

 

I only want to compile the mqx-libraries. And the following warning happens:

 

invalid project path duplicate path entries found

 

Can anyone help?

 

 

The following appears in the Problems window:

Description    Resource    Path    Location    Type

Invalid project path: Duplicate path entries found (/bsp_twrmcf52259 [Include path] isSystemInclude:true includePath:C:/Freescale/CW MCU v10.5/MCU/ColdFire_Support/ewl/EWL_C/include), path: [/bsp_twrmcf52259].    bsp_twrmcf52259        pathentry    Path Entry Problem

 

thanks

 

Ms. Piggy

Labels (1)
1 Solution
8,630 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi!

Check in menu Project > Properties > C/C++ Build > Settings > >ColdFire Compiler > Input and also menu Project > Properties > C/C++ Build > Settings > >ColdFire Linker > Input that you dont have duplicated include paths

If your problem persists I recommend to move to CW10.6 or submit a Service Request at www.freescale.com/support

Regards,

Carlos

View solution in original post

4 Replies
8,631 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi!

Check in menu Project > Properties > C/C++ Build > Settings > >ColdFire Compiler > Input and also menu Project > Properties > C/C++ Build > Settings > >ColdFire Linker > Input that you dont have duplicated include paths

If your problem persists I recommend to move to CW10.6 or submit a Service Request at www.freescale.com/support

Regards,

Carlos

8,630 Views
kleckerspur
Contributor III

It seems to work. There were duplicated pathes in  user- and system path.

If you have a lot of includes in the user path, it is very difficult to find out

Is there an easy way to find out which duoblicated items in there. or to save the whole stuff, to bring it restore it afterwards ?

0 Kudos
Reply
8,630 Views
kleckerspur
Contributor III

The problerm happens with 10.6

0 Kudos
Reply
8,630 Views
kleckerspur
Contributor III

Well then?

0 Kudos
Reply