invalid project path duplicate path entries found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

invalid project path duplicate path entries found

跳至解决方案
11,950 次查看
kleckerspur
Contributor III

Hello,

 

I only want to compile the mqx-libraries. And the following warning happens:

 

invalid project path duplicate path entries found

 

Can anyone help?

 

 

The following appears in the Problems window:

Description    Resource    Path    Location    Type

Invalid project path: Duplicate path entries found (/bsp_twrmcf52259 [Include path] isSystemInclude:true includePath:C:/Freescale/CW MCU v10.5/MCU/ColdFire_Support/ewl/EWL_C/include), path: [/bsp_twrmcf52259].    bsp_twrmcf52259        pathentry    Path Entry Problem

 

thanks

 

Ms. Piggy

标签 (1)
1 解答
8,649 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi!

Check in menu Project > Properties > C/C++ Build > Settings > >ColdFire Compiler > Input and also menu Project > Properties > C/C++ Build > Settings > >ColdFire Linker > Input that you dont have duplicated include paths

If your problem persists I recommend to move to CW10.6 or submit a Service Request at www.freescale.com/support

Regards,

Carlos

在原帖中查看解决方案

4 回复数
8,650 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi!

Check in menu Project > Properties > C/C++ Build > Settings > >ColdFire Compiler > Input and also menu Project > Properties > C/C++ Build > Settings > >ColdFire Linker > Input that you dont have duplicated include paths

If your problem persists I recommend to move to CW10.6 or submit a Service Request at www.freescale.com/support

Regards,

Carlos

8,649 次查看
kleckerspur
Contributor III

It seems to work. There were duplicated pathes in  user- and system path.

If you have a lot of includes in the user path, it is very difficult to find out

Is there an easy way to find out which duoblicated items in there. or to save the whole stuff, to bring it restore it afterwards ?

0 项奖励
回复
8,649 次查看
kleckerspur
Contributor III

The problerm happens with 10.6

0 项奖励
回复
8,649 次查看
kleckerspur
Contributor III

Well then?

0 项奖励
回复