internal compiler error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

internal compiler error

5,378件の閲覧回数
munteanufani
Contributor I

internal compiler error (report to <[email protected]>) while executing in file 'PCodeInfo.c' line: 2284

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

5,296件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Fani,

Could you tell us which CodeWarrior and MCU are you using? Are you running an example project? It would be helpful if you could give us more information.

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

5,296件の閲覧回数
munteanufani
Contributor I

I made a mistake: the board used is based on the K60 microcontroller.

Sorry.

0 件の賞賛
返信

5,296件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Fani,

 

Thanks for the information. Is there a specific reason for moving to CodeWarrior? If you are early in your design cycle on Kinetis devices  then you may choose to move to the MCUXpresso IDE:

http://www.nxp.com/products/software-and-tools/run-time-software/mcuxpresso-software-and-tools/mcuxp... 

Regarding the error, CodeWarrior has two compilers please make sure you selected the GCC compiler for your project which is the same compiler used by KDS:

pastedImage_2.png

Could you post the information shown in the console window about the error?

If you decide to use CodeWarrior I would also recommend you to use the latest CodeWarrior version which is 10.7:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

 

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

5,295件の閲覧回数
munteanufani
Contributor I

Hi Carlos,

We have two projects. The latest is based on FRDM-K64 / KDS / MQX4.2 derived from an old project based on K60 / CW 10.2 / MQX3.8. We've frozen this old project to this configuration, but we want to keep upgrading after the new project flow. When porting the same libraries on both projects, the old K60-based project generated this error. Each change in this project (K60 / CW 10.2 / MQX3.8) generates additional costs: CW license, change to other versions of MQX.

Regarding at this error is attached a capture with last info from CW’s console.

Thank you,

Fani M.

0 件の賞賛
返信

5,295件の閲覧回数
munteanufani
Contributor I

Hi Carlos,

I’m used a development board from freescale FRDM-K64F.

CodeWarrior for MCU Version: 10.2, Build Id:120126

I do not use an example project. It’s a more complex project. When I added a new library, this happened. On KDS the project is built with no errors and works well. If you need more information, please let me know. I attached a desktop capture.

Thank you,

Fani Munteanu

0 件の賞賛
返信