interface between K20D50M with a sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interface between K20D50M with a sensor

1,863 Views
sosopavliashvil
Contributor I

Hi all,

 

I am really new to microcontrollers. I am trying to interface K20D50M with a capacitance sensor. I was wandering if there are any demo projects that I can use.

Here is the serial data format of the capacitance sensor:

 

The ASCII output from TXD pin of J4 contains three fields: sequence number, measurement time (in seconds), and measured capacitance. The line format is as below.

SSSSS TTTTT.tt CCCCU

where ‘SSSSS’is 5 digit sequence number, ‘TTTTT.tt’is 8 digit time stamp (in second), and CCCCU is 5 digit measured capacitance with U being unit digit. Different fields are separated by 1 space. Each line is ended with ‘LF’(0x0A) and ‘CR’(0x0D). Output baud rate is 38400bps fixed. Data format is 8 data bits, 1 stop bit, and no parity.

Output level is 5V. So a level converter is needed to connect to RS232 compatible device (PC serial port, for example).


Could you please send me If you have any demo projects that would be helpful

Thank you and have a great day

Labels (1)
0 Kudos
Reply
1 Reply

1,811 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Please give a check to the answer provided in the next thread:

Kinetis K20D50M interface with Capacitance sensor

Regards!

Jorge Gonzalez

0 Kudos
Reply