how to get bareboard driver code (ex: USB, ethernet, PCIE ...) for P2020 and MPC8378?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to get bareboard driver code (ex: USB, ethernet, PCIE ...) for P2020 and MPC8378?

1,449件の閲覧回数
jingyibin
Contributor I

I use CodeWarrior V10.5.1 to debug my P2020 RDB, but I find that there is no bareboard driver for USB, ethernet and PCIE which I need to access to for my next-step debug. How could I find these bareboard driver?

0 件の賞賛
返信
1 返信

1,351件の閲覧回数
Pavel
NXP Employee
NXP Employee

There are no bare board drivers for the P2020 or MPC8378 USB, Ethernet or PCIe.

Look at recommended initialization sequence for USB, Ethernet and PCIe in the P2020 Reference Manual:

See the Sections 18.6.1 and 18.8.1 about USB initialization.

See the Section 14.6.3 about Ethernet and the Section 16.13 about PCIe.

 

Look at recommended initialization sequence for USB, Ethernet and PCIe in the MPC8379 Reference Manual:

See the Sections 20.6.1 and 20.8.1 about USB initialization.

See the Section 18.6.2.1 about Ethernet and the Sections 14.5 and 15.7 about PCIe.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信