how to create ELF file in codewarrior5.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to create ELF file in codewarrior5.2

2,624 Views
yikunliu
Contributor II

i want to use freemaster with codewarrior5.2 project.

but freemaster can't display variables and address when i load a MAP file.

i think ELF file is useful

how to create ELF file in codewarrior5.2  ???

3 Replies

2,446 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yikun liu,

How about the *.abs file ?

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,446 Views
yikunliu
Contributor II

it's useful !!!!

thank you verymuch~

0 Kudos
Reply

2,446 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Good to hear it worked.

BR

Alice

0 Kudos
Reply