flash tools wont work on s12zvmc128 with P&E Multilink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flash tools wont work on s12zvmc128 with P&E Multilink

1,590 次查看
tiberiusvanca
Contributor II

Hi there,

 

I use:

    - CodeWarrior for MCU
     Version: 10.6.4
     Build Id:150416

with an

P&E Multilink Universal RevC Debugger.

 

Now i want to use the secure flash option.

If i download my firmware with via Debug or Run, all works fine. I get a notice that the device is secure and to unlock i need to erase. Works like a charm.

 

As soon as i try to program that lovely cpu with CodeWarriors integrated flash tool, i get an error (see attachment).

I use the same connection as in the run configuration. It does not make any difference if secure the firmware or not. Flash tools simply wont work!

 

Also i have not found out yet were CW does save the connection properties.

 

Any help would be welcome.

 

Kind Regards

Clemens

Original Attachment has been moved to: support1.txt.zip

标签 (1)
2 回复数

1,441 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Clemens,

Cloud you please take a screenshot about the configure when you flash with " CodeWarriors integrated flash tool".

And whether it secured when you use the flash toll , so it can not write any registers .

BR

Alice

1,441 次查看
iggi
NXP Employee
NXP Employee

The topic will be moved to CodeWarrior space as it concerns the integrated flash programming tool (not  that much the MCU)

0 项奖励
回复